New Flagship Multi-Spectral Maritime Camera Systems
Tuesday - 28 October 2025
Fareham, UK: FLIR, global leader in high-performance marine thermal-imaging systems, announced today the debut of its new flagship series of multi-spectral maritime camera systems, the M460 and M560.
The M460 and M560 are elite AI-powered multi-spectral camera systems tailored specifically for professional marine applications ranging from first responders, commercial vessels, and superyachts. Taking the next step from a conventional thermal camera, the M460 and M560 are complete marine-imaging systems that combine a high-performance thermal sensor with a 4K, low-light visible camera, a 12KM ITAR-free laser rangefinder and long-range LED laser spotlight.
The new FLIR M460 and M560 cameras feature advanced FLIR AI Target Tracking that goes far beyond traditional systems. Using an onboard neural network, the cameras keep a watchful eye on the open water and automatically identify and classify common marine objects – like vessels, buoys, and people – for easy interpretation. Once an object is selected, the camera intelligently tracks the target with dynamic pan and tilt control, maintaining precision even in rough seas, crowded waterways, or during high-speed maneuvers.
To deliver reliable performance in any sea condition, the FLIR M460 and M560 feature the industry’s first three-axis gyro stabilisation system. This advanced technology compensates for pitch, roll, and yaw—ensuring smooth, distraction-free imagery and exceptional long-range image quality. It also enhances the accuracy of AI-powered target acquisition, even in the most challenging sea states.
“With the launch of the FLIR M460 and M560, we’re setting a new standard for maritime situational awareness,” said Grégoire Outters, General Manager of FLIR Marine. “By developing our own AI neural network specifically for the maritime environment and integrating it into these cameras, we’ve transformed the M460 and M560 into essential tools for tracking targets, reducing operator workload, and enabling smarter decision-making when it matters most. With advanced three-axis gyro stabilisation and multiple payload options, these cameras give mariners the confidence to navigate any situation on the water.”
For thermal imaging, the M460 uses a high-sensitivity, long-wave infrared (IR) thermal sensor to deliver best-in-class image quality along with improved contrast, spatial filtering and image sharpening. M460's thermal sensor is equipped with a 5x optical zoom lens for early detection of distant targets.
The M560 uses a high-sensitivity, mid-wave IR thermal sensor and 14x optical zoom lens to further enhance detection capabilities, image quality and deliver a long-range performance. Both cameras offer Colour Thermal Vision (CTV), combining the color visual elements from the visible camera to enhance and provide context to the thermal scene. With CTV, navigation marks appear in their natural red and green, while vessels and shoreline features are easier to identify with color overlays.
The M460 and M560 feature an integrated tight-beam laser spotlight with the ability to illuminate objects up to 1km away and enhance the 4K camera performance. Each model is also available to come pre-installed with or without an ITAR-free laser rangefinder designed to accurately measure target distance at long range and in less-than-ideal visibility conditions. Models with the rangefinder will offer an effective range up to 6.5 nautical miles (12km).
The M460 and M560 will be on display at the FLIR stand, 08.729 during METSTRADE, Nov. 18 – 20, 2025 at the RAI Amsterdam.
The new FLIR M460 and M560 cameras are available through FLIR's network of authorized dealers and distributors. For more information connect with a FLIR product expert.